Technical FAQs

Ask a Question

Does the ATS48 have a remote fault reset function?    

Issue:
Does the ATS48 have a remote fault reset function? 

Product Line:
ATS48

Environment:
All

Cause:
Need external reset by logic input.

Resolution:
Yes , Goto I/O menu ,
 Goto  LI3 / LI4 assignments 
Set to LIr  (external reset via logic input)
 
Was this helpful?
What can we do to improve the information ?