Technical FAQs

Ask a Question

How can an I-Line II busway run be separated in the middle ?

Issue:
Can an I-Line II busway run be separated in the middle? 

Product Line:
Busway

Environment:
I-Line 2

Cause:
Maintenance or Repair

Resolution:
 

Busway sections can be removed without disturbing adjacent sections of busway by removal of the joint pack.

Joint packs can be removed from the busway by loosening the 1/2" dia. torque bolt(s) as loose as possible without backing out of the nut retained on the opposite side and removing the #10 screws that hold the joint pack onto the busway duct top.

Lightly tap joint pack out from the side.

 

Was this helpful?
What can we do to improve the information ?