Technical FAQs

Ask a Question

Is the 82255 double throw switch CSA Certified?

Issue:
UL and CSA standards

Product Line:
Double throw safety switch

Applicaton:
82255

Cause:
Understanding the applicable standards met

Resolution:
The 82255 is marked cULus, which is a UL Listing for both Canada and the USA.

Was this helpful?
What can we do to improve the information ?