Technical FAQs

Ask a Question

What are the repair parts for the HU364, series F5? (may be shown as F05)

Issue:
The list of repair parts is needed for Safety Switch catalog number HU364, series F5.

Product Line:
Heavy Duty Safety Switch

Environment:
Applicable only to HU364, Series F5

Cause:
The repair parts numbers for the HU364, series F5, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

Resolution:
The repair parts for the HU364, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056703950 - (requires one per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Complete Line/Load Base mounting screws - 40205-464-01 (requires 6 per base)
Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - 40251-162-51 (per lug)
Lug Assembly mounting screw - 21401-222-40
Switch Mechanism - 40566-786-50
Switch Mechanism mounting screws- 22999-405-62 (requires 2)
Handle Assembly - 40566-635-50
Lockplate - 40566-721-01
Lockplate mounting screws - 22999-405-62 (requires 2)
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)

Was this helpful?
What can we do to improve the information ?