Technical FAQs

Ask a Question

What are the differences between options L09 and R09?

Issue:
Customer is asking to change from option L09 to option R09.

Product Line:
ATV61, E-Flex, 8839EFD

Environment:
All models

Cause:
None

Resolution:
L09 is Lonworks communication card.  R09 is Bacnet communication card. 

Was this helpful?
What can we do to improve the information ?