Technical FAQs

Ask a Question

What are the repair parts for a HOM12M100RB, Series S03 load center?

Issue:
Current design repair parts

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - 4056317850 (also called a Door)
Cover Mounting Screw - 2142217101 (2 Required)
Interior Trim with labels- 4056312702K (also called a Deadfront trim)
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056507351 (Interior assembly does not come with main breaker, see below Main Breaker) 
Interior mounting screws - 4020510001 (3-required)
Main Breaker - QOM100VH
Neutral Bonding Screw - 4028345850K
closing cap for top endwall - 4023000201
closing cap mounting screws - 2142720241 (2 required)
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?