Technical FAQs

Ask a Question

What are the repair parts for a HOM3040M200CEP, Series S03 load center?

Current design repair parts

Product Line:
Homeline load centers

repair parts



Only the parts listed below are considered field replaceable:
Cover - HOMC30UC
Cover Mounting Screw - 4020513002K
Cover Door Hinge - 4028356450K
Door Latch Kit 4020284450K
Interior Assembly - 4056508751 (interior assembly does not include the main breaker, see main breaker below)
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM2200VH
Standard Endwall plates with knockouts - 4028366350 (bag assembly includes the standard plates that come with the load center from the factory, along with instruction bulletin and insert card)
Shorter ground bar kit - PK9GTA
Longer ground bar kit with larger lug - PK15GTA and LK100AN  
Was this helpful?
What can we do to improve the information ?