Technical FAQs

Ask a Question

Can a JJA36250M75 breaker be ordered in a factory assembled I-Line panel ?

Issue:
Can a JJA36250M75 Mag Guard breaker be ordered in a factory assembled I-Line panelboard?

Product Line:
I-Line Panelboards sold and supported in the USA. 

Environment:
Application

Cause:
Offering

Resolution:
Because the panel does not have a UL508 rating , we cannot supply a magnetic only breaker in this panelboard from the factory . The panel is UL67 rated instead. MAG-GARD I-Line breakers are usually associated with I-Line OEM panels .

Was this helpful?
What can we do to improve the information ?