Technical FAQs

Ask a Question

XCSE identification

Directed to Safety Interlock catalog online and directed Customer to look on side of switch for identification.

Issue:
All stock numbers and specifications of Preventa Interlock Switches product are not published in Digest 176; customers are unsure where to find additional specification and rating information.

Product Line:
All Preventa Interlock Switches

Environment:
US product

Cause:
Customers are unsure where to find stock numbers and specification and rating information if it is not in Digest 176

Resolution:
Additional information about ratings and specifications can be found in Preventa Interlock catalog which can be downloaded here:

http://download.schneider-electric.com/files?p_File_Id=340559564&p_File_Name=MKTED208051EN-US-Rev.-01-Chapter-4-.pdf
 

Was this helpful?
What can we do to improve the information ?