Technical FAQs

Ask a Question

Cable Pull Switches XY2CE2A2968H7 and XY2CE4A010 general info

Directed to Cable Pull Switch Catalog online.

Issue:
All stock numbers and specifications of Preventa Pull Switches product are not published in Digest 176; customers are unsure where to find additional specification and rating information.

Product Line:
All Preventa Pull Switches

Environment:
US product

Cause:
Customers are unsure where to find stock numbers and specification and rating information if it is not in Digest 176

Resolution:
Additional information about ratings and specifications can be found in Preventa Pull Switch catalog which can be downloaded here: 

http://download.schneider-electric.com/files?p_File_Id=454779757&p_File_Name=MKTED208051EN-US-Rev.-02-Chapter-6.pdf

Was this helpful?
What can we do to improve the information ?