Technical FAQs

Ask a Question

XCKT2118G11

Directed to Online catalog 9007CT0501 for specifications (page 2 & 67)

Issue:
All specifications of XC Limit Switches product are not published in Digest 176; customers are unsure where to find additional specification and rating information.

Product Line:
All XC Limit Switches

Environment:
US product

Cause:
Customers are unsure where to find specification and rating information if it is not in Digest 176

Resolution:
Additional information about ratings and specifications can be found in XC catalog which can be downloaded here:  http://download.schneider-electric.com/files?p_Doc_Ref=9007CT0501

Was this helpful?
What can we do to improve the information ?