Technical FAQs

Ask a Question

What are the dimensions of the 9049ER

Issue:     
What are the dimensions of the 9049ER

Product Line:
Pressure Switches

Environment:
9049 Pressure Switch accessories

Cause:
Dimensions of the 9049ER
 
Resolution:
The rod is .187 (3/16") in diameter and the threading is #10-32 for 3/8" on each end.

Part Number Length (in)
9049ER1 1.75
9049ER2 2.5
9049ER3 3.5
9049ER5 5.25
9049ER7 7.25
9049ER12 12.25


Was this helpful?
What can we do to improve the information ?