Technical FAQs

Ask a Question

Is the 9037HR NEMA 7 and 9 rated?

Issue:     
What is the Nema enclosure rating on the 9037HR closed tank float switches?

Product Line:
Pressure Switches

Environment:
9037HR Pressure Switches

Cause:
Is the 9037HR NEMA 7 and 9 rated? 

Resolution:
This device is UL listed as UL508 for industrial control and UL698 for hazardous locations.
Was this helpful?
What can we do to improve the information ?