Technical FAQs

Ask a Question

Can class 9012 type GCW be used for air pressure instead of water?

Issue: 
Can class 9012 type GCW be used for air pressure instead of water?

Product Line:
Pressure Switches

Environment:
Class 9012 type GCW limit switches

Cause:
Need a pressure switch for gaseous bodies.
 
Resolution:
The class 9012 type GCW switch were developed for hydraulic fluids and as a general rule was not desiged to be used for gaseous bodies as they have never been tested for this use.
Was this helpful?
What can we do to improve the information ?