Technical FAQs

Ask a Question

Should the Type ML limit switches be used in applications where they will be operated under an oil or coolant spray?

Issue: 
Should the Type ML limit switches be used in applications where they will be operated under an oil or coolant spray?

Product Line:
Limit Switches
 
Environment:
Limit Switches

Cause:
Should the Type ML limit switches be used in applications where they will be operated under an oil or coolant spray?
 
Resolution:
Unbooted versions of the type ML limit switches should not be used in this type of application

Was this helpful?
What can we do to improve the information ?