Technical FAQs

Ask a Question

What are the UL and CSA file numbers for the 9070T control transformers?

Issue:
What are the UL and CSA file numbers for the 9070T control transformers?

Product Line:
OEM Safety/Controllers

Environment:
9070 control transformers sold and supported in the USA.

Cause:
UL and CSA file numbers for 9070T control transformers.

Resolution:
The UL file is E61239, Guide XPTQ2 from 25 to 5000 VA.
 
The CSA file is LR37055, Guide 184-N-90 from 25-5000 VA.  


 
Was this helpful?
What can we do to improve the information ?