Technical FAQs

Ask a Question

What are the repair parts for a HOM40L200RB, Series S03 load center?

Issue:
Current design repair parts

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317250 (Includes hinges attached to left side of cover)     
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056314201K            
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056514151 (interior assembly does not come with main lugs, see below main lugs kit) 
Main Lugs Kit - QOL225
Neutral Bonding Screw - 4028345850K
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?