Technical FAQs

Ask a Question

What are the repair parts for a HOM30L200RB, Series S03 load center?

Current Design repair parts

Product Line:
Homeline load centers

Repair parts


Only the parts listed below are considered field replaceable.
Cover - 4056317450 (Includes hinges attached to left side of cover)  
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056313801K
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056508651 (Interior assembly does not include the main lugs, see below main lug kit) 
Main Lugs Kit - QOL225
Neutral Bonding Screw - 4028345850K
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?