Technical FAQs

Ask a Question

Can you replace a ATS48 with a ATV drive inside an existing enclosed 8639 48U soft starter unit?

Issue:
Can you replace a ATS48 with a ATV drive inside an existing enclosed 8639 48U soft starter unit?

Product Line:
8639 48U soft starter

Environment:
All

Cause:
Soft starter replacement with an drive?

Resolution:
This would not be feasible. We don't have a parts list or instructions/kit to change from a soft start to a drive. They are two different type of units. Recommend ordering the correct enclosed drive unit to get all the UL listed and tested components.
Was this helpful?
What can we do to improve the information ?