Technical FAQs

Ask a Question

How can electrical noise on the +10v DC be reduced?

Issue:
RF noise is causing an unstable speed.

Product Line:
ATV66

Environment:
All models and serial numbers.

Cause:
None

Resolution:
Connect a jumper wire between the common terminal (COM) should be connect to ground at one point in the control system.

Was this helpful?
What can we do to improve the information ?