Technical FAQs

Ask a Question

How can I order an M-Flex for a constant torque application come in a Nema 3r?

 

 Issue:
How can I order an 8839 M-Flex for a constant torque application in a Nema 3R?

Product Line:
8839MFD

Environment:
All

Cause:
Application is constant torque

Resolution: 8839 MFlex does not offer nema 3R enclosures.   Nema 3R only available in 8839 EFlex (variable torque only).
For custom 3R enclosure with an ATV71 consult  Schneider Electric Field Office.
Was this helpful?
What can we do to improve the information ?