Technical FAQs

Ask a Question

What is the terminal lug data for an EZM31200FST, EZM11200FST, EZM31200FSB or EZM11200FSB?

Issue:
Lug wire range

Product Line:
EZM

Environment:
1200A Main FS

Cause:
Assure wire purchased is compatible

Resolution:
The terminal lugs will accept up to (4) #3/0 AWG - 500 KCMIL conductors per phase and neutral.



Was this helpful?
What can we do to improve the information ?