Technical FAQs

Ask a Question

Can the tank-connecting bushing and float on the 9037 type H float switches be removed in the field?

Issue:
Can the tank-connecting bushing and float on the 9037 type H float switches be removed in the field?

Product Line:
Float Switches

Environment:
Closed Tank Type H Float Switches

Cause:
Product Adaptation

Resolution:
Yes, both the float and the tank-connecting bushing can be removed in the field. Alternatively, to purchase the item with these modifications use form F3 (to omit tank-connecting bushing) or form L (to omit float).
Was this helpful?
What can we do to improve the information ?