Technical FAQs

Ask a Question

Can the wireless button in the factory paired non-programmable packs be replaced?

If a non-programmable push button is damaged, can it be replaced?

Product Line: 
XB5/ XB4 Harmony

XB5/ XB4 Harmony wireless push button

Clarify if any of the non-programmable components be replaced.

No replacements are available.   There is no way to program the receiver to accept another transmitter.   If any component is damaged, both parts need to be replaced.

Was this helpful?
What can we do to improve the information ?