Technical FAQs

Ask a Question

Can the wireless push button be used in a emergency stop application?

Issue: 
Can the Harmony wireless pushbutton be used in an emergency stop application?

Product Line:
Harmony

Environment:
Harmony wireless push button 22mm

Cause: 
Clarify if wireless push buttons can be used as a emergency stop application. 

Resolution: 
All emergency stop applications must be hardwired.  The Harmony wireless push button should not be used in any critical application.

Was this helpful?
What can we do to improve the information ?