Technical FAQs

Ask a Question

If I order two 9001KS53K5's, will the keys be the same?

Issue: 
When ordering 9001KS**K* keyed operator, will they all come with the same keys

Product Line: 
9001KS

Environment:
Nema 4, 30 mm keyed selector switches

Cause: 
Serveral different keys are needed for an application, restricting access to only certain personnel

Resolution: 
When ordering 9001KS**K* keyed operators, they will all come standard with the E10 key.  Must specify at end of part number with a different E11 - E99 key code

Was this helpful?
What can we do to improve the information ?