Technical FAQs

Ask a Question

XW Recharge Volts.

                                                                                                                                  XW Recharge Volts


Sets the battery voltage level at which a new charge cycle begins. Recharge Volts
is automatically temperature compensated to be consistent with the charge voltage
which is also temperature compensated.
When using Grid Support/Sell, during evening hours, unless Load Shave is enabled, the XW will be in AC Pass Thru, and will
consume approx 30W just to stay powered from the battery.
Recharge Volts needs to be set at least 2V lower than GSV to avoid repeated charge cycles during non-solar hours and at least 2V higher than LBCO to avoid
nuisance low battery warnings.
Was this helpful?
What can we do to improve the information ?