Technical FAQs

Ask a Question

Can a NEMA Type 1 safety switch be converted in the field to NEMA Type 3R?

Issue:
Conversion of Type 1 to Type 3R

Product Line:
General Duty Safety Switches
Heavy Duty Safety Switches
Double Throw Safety Switches

Environment:
All HD, GD and DT switches

Cause:
Incorrect device purchased

Resolution:
No, it could not be converted. The customer would need to purchase the correct switch for the application.
Was this helpful?
What can we do to improve the information ?