Technical FAQs

Ask a Question

GT250 L/R Matrix Gate FXX50/51

Matrix Gate Fault can be caused by one or more of the following:
 
  • Fiber-optic harness is loose or disconnected
  • CCU2 ±15 Vdc Power Supply is defective
  • P1 on driver board is loose or disconnected
  • Blown matrix (IGBT or cap)
Was this helpful?
What can we do to improve the information ?