Technical FAQs

Ask a Question

What is the part number for a hand-auto switch on an enclosed ATV66 drive?

Issue:
Selector switch replacement


Product Line:
ATV66 Enclosed


Environment:
Type 1 & 12


Cause:

None

Resolution:
The part number we used was ZA2BD2, but this is now obsolete.  The new part to replace it with is XB5AD21 which is a complete operator that includes a 2 position selector, mounting collar and contact block. 
Was this helpful?
What can we do to improve the information ?