Technical FAQs

Ask a Question

Is the QUM400CK, Series M02, provided with a factory installed service disconnect?

Issue:
Determine if a main breaker is provided

Product Line:
Combination Service Entrance Device (CSED)

Environment:
All single main 400A CSED

Cause:
Determine if a main is required to be ordered separately.

Resolution:
Yes, an LJL36400U31X circuit breaker is supplied factory installed.
Was this helpful?
What can we do to improve the information ?