Technical FAQs

Ask a Question

What is the terminal lug data for the LJL36400U31X main breaker provided in a QUM400CK, Series M02 Combination Service Entrance Device?

Wire size range

Product Line:
Combination Service Entrance Device (CSED)

Wiring components

Needs to know the wire range of the breaker lugs

The load side lugs of the main breaker are suitable for use with (2) 2/0 - 500 KCMIL AL/CU conductors per phase.
Was this helpful?
What can we do to improve the information ?