Technical FAQs

Ask a Question

What is the difference between a ZBA5 and a ZBA75 lens caps?

Issue:
What is the difference between a ZBA5 and a ZBA75 lens caps?

Product Line:
22mm push buttons

Environment:
XB5 operators

Cause:
Product features and verification

Resolution:
The ZBA5 is for the standard ZB5 push button and the ZBA75 is for the ZB5R wireless pushbuttons.
The design and mounting is different between the two and they are not interchangable. 

Was this helpful?
What can we do to improve the information ?