Technical FAQs

Ask a Question

What is the part number of the end closing plate used on old style EZM equipment that measures 6.5" W x 9.5" H?

Issue:
Part number request

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The part number is 40528-317-50, but it is obsolete and no longer available.
 

Was this helpful?
What can we do to improve the information ?