Technical FAQs

Ask a Question

When working with EZM equipment, can the need for a transition section be determined without knowing the catalog number of the existing equipment?

Identify equipment

Product Family:
EZM Multi Metering

Adding to existing equipment

Assure correct equipment is provided

Yes, an "old style" piece of EZM equipment can be identified by looking at the end closing plate that can be found at either end of the equipment lineup. The old style EZM equipment end closing plate would measure approximately 6.5" W x 9.5" H. The current style of EZM equipment end closing plate would measure approximately 5" W x 17" H.

Was this helpful?
What can we do to improve the information ?