Technical FAQs

Ask a Question

What is the coil part number for the 8536 starters?

Issue:
8536 coil are available in different voltages. What are the part numbers?

Product Line:
Starters

Environment:
Applies to NEMA starters only.

Cause:
8536 coil are available in different voltages. What are the part numbers?

Resolution:
See attachment.
 

Was this helpful?
What can we do to improve the information ?