Technical FAQs

Ask a Question

Where can you find information on the wire sizes for Powerguard ATV61/71?

Issue:
Where can you find information on the wire sizes for Powerguard ATV61/71?

Product Line:
ATV61 and ATV71

Environment:
All serial numbers for ATV61 and ATV71

Cause:
For how to size wires for the drive

Resolution:
Information for maximum wire sizes can be found in the INstruction Bulletin for the Altivar 61//71 Powerguard 18 Pulse Adjustable Speed Enclosed Drive.  The current document number is 30072-451-53 and it can be downloaded from the Schneider Electric USA website.
Was this helpful?
What can we do to improve the information ?