Technical FAQs

Ask a Question

What is the SIL rating XCSPA593?


Issue:
SIL ratings are not published in Digest 176, customers are unsure where to find the information.

Product Line:
Preventa Safety Solution Equipment

Environment:
US product

Cause:
SIL ratings are sometimes necessary for quotations; they are not published in Digest

Resolution:

Can reach SIL 3 with the appropriate monitoring system and correctly wired conforming to EN/IEC 61508.


 

Was this helpful?
What can we do to improve the information ?