Technical FAQs

Ask a Question

Can an ATV56 program be transferred to an ATV61?

Issue:
Can an ATV56 program be transferred to an ATV61? 

Product Line:
ATV56 Altivar 56

Environment:
All

Cause:
Replacement Drive

Resolution:
No, a process to transfer a parameter file from ATV56 to ATV61 is not available.  Manually input parameter settings to the ATV61.
Was this helpful?
What can we do to improve the information ?