Technical FAQs

Ask a Question

What are the repair parts for a HOM4252M200C, Series S03 load center?

Issue:
Current design repair parts

Product line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Cover - HOMC42UC
Cover Mounting Screw - 4020513002K
Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Interior Assembly - 40565-918-51 (Interior assembly does NOT include the main breaker, see below main breaker)
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM2200VH
Was this helpful?
What can we do to improve the information ?