Technical FAQs

Ask a Question

What can cause the motor to run from an E-Flex when the AFC/OFF/BYPASS switch is in AFC and the HAND/OFF/AUTO is in OFF?

The E-Flex is running the motor when it should not.

Product Line:

All models with bypass

The drive has a RUN command when HOA is OFF. 

Typically, the run command is applied to logic input LI1.  Verify that LI1 is high and then troubleshoot both the 24Vdc and 120Vac control circuits.  
Probable causes include miswiring, failed relay, induced voltage, and failed HOA switch/contact.
Was this helpful?
What can we do to improve the information ?