Technical FAQs

Ask a Question

ATS48 without a shorting contactor. Is it ok to install a current sensor on the output of the Softstart.

Issue:
Install a current sensor on the output of ATS48

Product line:
Altistart 48, ATS48

Environment:
All models, all serial numbers

Cause:
Need to monitor current and activate an output.

Resolution:
It is ok to use motor current sensor on the output of the softstart. Also, motor underload feature built-in to the softstart can be used to activate a Logic output.

Was this helpful?
What can we do to improve the information ?