Technical FAQs

Ask a Question

What is the part number for the multi-loader?

Issue:
What is the part number for the multi-loader?

Product Line:
All

Environment:
All

Cause:
Configurataion tools

Resolution:
The Multi-loader part number is VW3A8121.
The multi-loader is used to copy a drives program from a device or SoMove lite via SD card and transferring to another drive or to a PC.

You can use the multi-loader on the following drives and soft starters:
ATV12, ATV312, ATV212, ATV32, ATV61, ATV71 and ATS22.

Was this helpful?
What can we do to improve the information ?