Technical FAQs

Ask a Question

How do you access the interior of the QO200TR to wire it.

Issue:
Access for wiring

Product Line:
AC Disconnect

Environment:
Access for wiring

Cause:
Needs to understand how to access the interior

Resolution:
When the outer cover is raised, you will see a single screw that is in the bottom right side corner of the deadfront. When this screw is removed, merely pull up on the outer enclosure. In one motion, you will be removing the cover, the top and side walls and the deadfront, exposing the interior of the device.





Was this helpful?
What can we do to improve the information ?