Technical FAQs

Ask a Question

Is the U3V1031BCR a top feed or bottom feed device?

Issue:
How to set up the device for incoming conductors.

Product Line:
Meter Socket, Vertical

Environment:
Installation requirement

Cause:
Understand direction of incoming service feed.

Resolution:
This 3 gang vertical meter stack is set up for overhead feed only. There will be an A-Type hub opening in the top endwall for conduit entry through 2.5".




 
Was this helpful?
What can we do to improve the information ?