Technical FAQs

Ask a Question

Can the VW3A1101 keypad display timeout on an ATV212 drive?

Issue:
Display timeout

Product Line:
Altivar 212, ATV212

Environment:
All Models and serial numbers

Cause:
None

Resolution:
It is not possible to have the display timeout on this ATV212 drive.

Was this helpful?
What can we do to improve the information ?