Technical FAQs

Ask a Question

Can more neutral space be added to a HCP36868M than what is provided in an HCW8SN ?

Issue:
Increasing neutral size

Product Line:
Panelboards

Environment:
I-Line

Cause:
Modification to existing

Resolution:
Another neutral or even a ground bar of the appropriate size can be added provided a local inspector is ok with  a hard wire connection from the existing neutral to that second one

Was this helpful?
What can we do to improve the information ?