Technical FAQs

Ask a Question

On a SDGT30020, which one of the 3 lugs are the 300 kcmil lugs and which is the 2/0 AWG lug?

Issue:
Understanding lug arrangement

Product Line:
Aux Gutter Tap Kits

Environment:
Riser applications

Cause:
Rise application

Resolution:
The 300 kcmil lugs are on the top right and bottom right. The 2/0 AWG lug is on the top right.
Was this helpful?
What can we do to improve the information ?