Technical FAQs

Ask a Question

XW AGS Max Run Time

Max Run Time is designed to allowed the generator to run for a specified time period and is designed to keep the generator from running out of fuel. 
With newer firmware, Max Run Time can be set up to 24 hrs. Once Max Run Time is reached the AGS will stop the generator, requiring the user 
to press ENTER (on SCP) to reset.
Was this helpful?
What can we do to improve the information ?