Technical FAQs

Ask a Question

Can the VW3A1101 HMI be backward compatible with all ATV61 and ATV71 drives?

Issue:
Compatibility of VW3A1101

Product Line:
ATV61, ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
The VW3A1101 HMI keypad is backward compatible with all ATV61 and 71 drives.

Was this helpful?
What can we do to improve the information ?